the code used to be working fine compiled with CCS3.1, not I have just moved the project to CCS6.1, most of the code is working fine, except the hardware interrupts.
in my main program I set it up like this:
IRQ_enable(IRQ_EVT_EXTINT4);
IRQ_globalEnable();
but later in one task IRQ_test(IRQ_EVT_EXTINT4) always returns zero, and the HWI ISRis never called.
The chip I am using is DM642. DSP/BIOS version 5.24, CSL version 2.31