Hello! when i use the USB of C6748 ,i found the example USB_DEV_BULK is too simple to satisfy my project. I need to auto send data to PC when the FIFO is full which is sized when configration. but your example just only use function of USBDBulkInit,without the arguments to config the FIFO the endpoints and DMA,rather than the outo mode.I want to config the registers ,but the work is complicate. SO, can u give me some advice to conplete my peoject ,and give me some examples both the C6748 and the PC,and give me files.
Thank you!
Have a nice day.