Hi,
Regarding to the DDR Bootloader configuration I was able to load /run a small application ( some section of section of it placed in DDR at run time so i assumed that the ddr problem solved . But when i shift to andother big project and use the same procedure ( Using AIS and check the ini file of it and burn it using flash burner ) my project not run after power up . Is it an initialization problem or not and how can i solve it .attached the Bios configuration of the two projects and the memory map also the ini file of the AIS C642x.ini