We have made our own board in which we are connecting FPGA and DSP TMS320C6455 . We have successfully download program in FPGA and in DSP we check all result using SdConfigEx software and we are using xds510usb emulator but while connecting in code composer studio 3.3 we get below error.
Error connecting to the target:
Error 0x80000240/-1146
Fatal Error during: Initialization, OCS,
Invalid data was scanned by the emulation controller.
Verify the board setup to make sure the scan chain is properly
defined.
If the setup is correct, then RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emu reset and reconnect to each target.
RESETSTAT pin of DSP is remain low and clkin1 and clkin2 are perfect 50Mhz and 25Mhz respectively and SYSTEMCLK3 output frequency is 25Mhz but i need 62Mhz.
so please help to solve this problem. It's urgent. please