I have Experience on working with Dm6437 and CCS_v3.3.
I am trying to work with DM 6437 with the TI IDE CCS_v6, I did all the setup for CCS _v6 to work with Dm6437 familiarize with non real time project now am facing problem on real time project.
I did the following things With CCSv6,
- Try to create new ccs project that is already exists in ccsv3.3 ie GPIO configuration LED project.
- Copy the same source code's.
- Added all necessary header and library files to project.
- compiled it then got error I resolved all.
- .out file is generated then I load that .out file to target without any errors.
- finally the code is running but the affect is not visible on board ie LED's are not blinking.
- I attached the snapshot for your reference.