Hi,
I have old project running on CCS 5.4 with MCSDK 2, now I am porting the old project to CCS 6.1 with MCSDK 3.
I defined TSCL as "extern volatile unsigned int cregister TSCL" but when I want to assign it to uint32_t variable = TSCL in the same file, I got error as "Symbol 'TSCL' could not be resolved"
I did not get this error when I compile with the old project with old CCS. I think it's may has something to do with compiler or linker or target......
I am choosing device 66AK2H12 with compiler TI v8.1.0. C6000 Linker
v/r
Yoyo