Hello, I'm writing a emifa driver which transfer data using edma3 (event (using gpio event ) trigger )based on the IOM mini-driver,my environment is as follows:
TMS320C6455DSP
V5 FPGA(interface with DSP using FIFO through emifa CE2)
CCS5.3
DSP/BIOS 5.42
EDMA3LLD
I have configured the emifa, edma3 and gpio,and I have found that the gpio event has triggered the edma3 transfer,because I set breakpoint in the edma3 transfer complete ISR,and the program is break at that ISR function, but if I look the EMIFA memory space,the ccs will pop up an error, which show the device core is hung ,and unable to determing target status,then it will disconnect with the target, and I can't find the reason,can someone give me some advice, thank you!