Hello
I use the LCDK6748 development kit, and I try to run the audio example:
\pdk_C6748_2_0_0_0\biospsp_03_00_01_00\drivers\examples\evm6748\audio
for this project there is no CCS project, the only example that include CCS project is th I2C example.
I try to create new project like explained in video:
C6748_BIOSPSP_CCSProjectCreation.wmv
and copy all files from example to the new created project folder. this include the folders:bin, obj, src
when I try to complie the project the linking fails :
<Linking>
"../obj/c6748-evm/c6xdsp/release/evm6748_audio_sample_configuro/linker_mod.cmd", line 37: error:
IROM memory range has already been specified
"../obj/c6748-evm/c6xdsp/release/evm6748_audio_sample_configuro/linker_mod.cmd", line 37: error:
IROM memory range overlaps existing memory range IROM
"../obj/c6748-evm/c6xdsp/release/evm6748_audio_sample_configuro/linker_mod.cmd", line 38: error:
IRAM memory range has already been specified
"../obj/c6748-evm/c6xdsp/release/evm6748_audio_sample_configuro/linker_mod.cmd", line 38: error:
IRAM memory range overlaps existing memory range IRAM
...
Is this is the way I need to build the project, or do I need to build it differently?