TI posts an object library for the Opus CODEC on the 66x platform. I want to port the code to the 6455 DSP so I will need the source code. I can get the source from opus-codec.org but their support for the TI DSP c6x platforms is not ready to be included in their normal source code distribution. It appears they have several macros defined that can be replaced with intrinsics. There also may be some loop unrolling to be done. Is the source code for the Opus CODEC available from TI?
dave