Hey,
We are using theTMS320C6748. The datasheet says that USB0_VDDA12 must be connected to a 0.22uF capacitor - table 3.32 in the datasheet.
However the checklist here says that if both USB ports are not used then the pin should be a no connect - http://processors.wiki.ti.com/index.php/OMAP-L13x_/_C674x_/_AM1x_Schematic_Review_Checklist#USB
This is an avionics design that was done year or two ago and the original datasheet said to leave the pins unconnected. We are finishing verification and have just seen the updated datasheet.
Can you tell me if the datasheet is correct or the checklist?
Cheers
Calum