Dear Ti:
I have a problem that how can i set my PLL frequencies. I set the PLL0_PLLM to a high value but my program can't run correctly. Now the setting is 18, which can set the pll0 to 456Mhz , it work good. but when i set it more than this num, like 23 in my .gen file, it will never run correctly.
but as the manual said,when my oscin is 24M, it can frequency doubling to 600MHZ