Hi,
In C6748 datasheet, I found below info are conflicted.
From below, it seems max 6 channel of PWM can be support on eHRPWMs.
From below, it seems max 4 channel of PWM can be support on eHRPWMs.
In C6748 TRM, it says each ePWM module can support up to 2 pwm outputs. As there is two eHRPWM modules on C6748, I think max 4 channel PWM to be support on C6748 eHRPWMs is correct info. Would you pls help to confirm?