Other Parts Discussed in Thread: OMAPL138
Dear Forum
we are developing owr board with C6748.
Some doubt about boot process :
1)In the Dev Kit, but also in other schematic, is present a NAND Flash of 4Gb , 16 bit ..The MT29F4G16xxx
It is connect with EMIF interface.This require a lot of pin.
Question is: what is the avantage/disadvantage to use a SPI NAND flash ,that require only some 3 pin ?
There is some BOOT performance to consider ?
2)When we will have owr board, the NAND will be connect, with no possibility to disconnect.
Question is: how do we update the BOOT contents ? There is a way via JTAG and owr Emulator
USB560 Blackhawk ?
3)And of course: how do we programm the first time the NAND with boot contents ? Do we need to
buy a flash programmer ?? What ?
Thanks for your time, and excuse for this maybe to simple questions?
Roberto