Hi,
In our design there is already a connection from C6747 to an UART, starting with both EMA_BA:
EMA_BA[0] to A[0], EMA_BA[1] to A[1], EMA_A[0] to A[2] and so on. This is working.
I want to make a further connection to an SRAM (MT48LC16M8A2) with the same 16 bit data at EMIF A. In SPRUFL6D.EMIF.PDF I can see at page 26, that in case of 16 bit data A[0] should be connected to EMA_BA[1] and A[1] to EMA_A[0] and so on, but there they are talking about asynchronous RAM.
In an example from Spectrum Digital I find an 1-to-1 connection (A[0-12] and BA[0-1]).
I got confused about starting with EMA_BA (one or both bits) or EMA_A[0]. If I must change our existing connection, I'll got in trouble with the existing UART. Hopefully I can connect to the SRAM starting with EMA_BA[0-1] like before, but SPRUFL6D.EMIF.PDF says this is for 8 bit data and asynchronous interfaces.
Kind regards,
Pablo H.