Other Parts Discussed in Thread: D810K013DZKB400, D810K013DZKB456, DA8XX
Hi,
The title shows that the part number is C6747, but in fact, DA810.
456Mhz part of DA810, running at 456Mhz, requires 1.3V (nominal) for CVDD, but does 456Mhz part, running at 400Mhz, require the same voltage ? I`m wondering if 1.2V might be enough to meet its operation condition. My customer is using 400Mhz part in their product, but because of its supply shortage, they are considering replacing 400Mhz part with 456Mhz one *without* HW/SW changes. I saw some specific AC timing parameters only for 456Mhz part in the datasheet. For example, EMIFB timing is different from 400Mhz part and 456Mhz one. Is AC timing of 400Mhz part applicable for 456Mhz part running 400Mhz ?
Best Regards,
Naoki