This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320C6747: Unable to create example mcasp project

Part Number: TMS320C6747
Other Parts Discussed in Thread: CCSTUDIO, SYSBIOS

Tool/software: TI-RTOS

Hi,

I am trying to compile mcasp example using pdksetupenv.bat and pdkProjectCreate.bat files, But while creating project facing an error . Please help me to resolve this issue

I have installed CCS version as : 5.3.0.00090

=========================================================================
Configuration:
   SOC             :   OMAPL137
   BOARD           :   all
   ENDIAN          :   little
   MODULE          :   mcasp
   PROCESSOR       :   dsp
   PDK_SHORT_NAME  :   C:\ti\PDK_OM~1\packages\
=========================================================================
Checking Configuration...
Complete
=========================================================================
GGR
C:/ti
   PDK_PARTNO         : OMAPL137
   PDK_ECLIPSE_ID     : com.ti.pdk.omapl137
   RTSC_PLATFORM_NAME : ti.platforms.evmOMAPL137
   RTSC_TARGET        : ti.targets.elf.C674
   CCS_DEVICE         : "com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"
*****************************************************************************
Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_OM~1\packages\\MyExampleProjects
Detected Test Project: MCASP_Audio_evmOMAPL137_c674xExampleProject

--------------------------------------------------------------------------------
Creating project 'MCASP_Audio_evmOMAPL137_c674xExampleProject'...

  !ERROR: Unknown RTSC product-type ID 'com.ti.pdk.omapl137'!
    NOTE: Refer to the following list of available RTSC product-type IDs (the display-names in square brackets are for reference only):

        ti.mas.dsplib.c674x [DSPLIB C674x]
        com.ti.sdo.edma3 [EDMA3 Low Level Driver]
        com.ti.rtsc.IPC [Inter-processor Communication]
        com.ti.rtsc.SYSBIOS [SYS/BIOS]
        com.ti.uia [System Analyzer (UIA Target)]
        com.ti.rtsc.XDAIS [XDAIS]
        com.ti.pdk.k2g [k2g PDK]

Copying macros.ini
The system cannot find the path specified.
        0 file(s) copied.
No projects detected
Project generation complete
*****************************************************************************