Hi,
I am doing an Active Noise Cancellation project. My requirements are similiar to another question, here is the link:
except that I have a specific process time requirement:
The first path in our program is 3m away from the quiet zone. The sound speed in air is around 340m/s so we have to finish the process in 8 msec.
We prefer to use LCDK to finish our project.
So my question is:
(1) Is the kit fast enough to finish the transmition and processing in 8 msec?
(2) How to solve the input problem? The board has 1 line in and 1 mic in. My project need two real time mic inputs. Can we make it on this board?
If the LCDK can't meet the requirements, can you recommend another for this project?
Thanks for your support and hoping to receive a reply from you soon.
Regards,
Li.