Tool/software: TI-RTOS
Hi All,
I Use a TMS320C6748 Custom Board,
Spi0 is configured in slave mode 4pin with CS in interrupt mode, the SPI driver is based on pspdrivers_01_30_01.
I try calling GIO_Read from within my "CommRX_TASK" seems that GIO Read is Blocking the hole system(CommRX_TASK is forever running),
lower priority tasks are not called till the master is sending some data.
isn't GIO read supposed to block and pend on a semaphore and release the system to handle some low priority tasks ?
can any one propose a reason in which GIO Read is Blocking other threads ?
Alex.