during my Jtag test, i faced a ID code error message. What can be the reasons?
My engineer told me that may be due to an old version on TMS32C6713GDPA200. Is this so?
Justin,
Can you post a screen shot of the error you are facing and the details of the setup (What emulator, version number of the device, etc) for us to better understand the problem. At this point it appears unlikely that a old version of the device should cause the issue but we can look at it once you provide the details.
Regards,
Rahul
---------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------
hi Rahul
TMS32C6713BGDPA300
We have present Version : D11.
NEXT: Is there a different bet 6713 & 6713B ? especially
J TAG : ID code test : FAILED
Data mismatched on device U3:
Actual data received: 0101 0000000001010111 00000010111 1
Expected data : 0011 0000000001010111 00000010111 1
Likely casue of failure:
Bad BDSL or Topology file
for my ICT test & J tag test?
Can you provide the file when you do a memory dump of the 6713.
There are silicon differences between the 6713 & 6713B which are specified in the 6713 Silicon Errata on the 6713B Webiste
-Drew
_____________________________________________________________________________
If the response answers your forum question: Please Verify Answer to alert others.
Are you aware of the TI Processors Wiki? This is a good place to search for additional support on TI ARM+DSP Application Processors.