This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMDSLCDK6748: SPI 0 communication

Part Number: TMDSLCDK6748

I am using a  TMDSLCDK6748  evaluation board. I want to configure the SPI communication in the board using SPI0 communication. But only the SPI0_SIMO, SPI0_SOMI and SPI0_SCLK pins are available in the J15 there is no chip select pin out from any of the output jumpers. They seem to be connected to the LAN IC, U23, LAN8710A-EZK.  SPI1 communication is available and seems to be connected to the camera header. 

Please suggest a way to use the SPI communication in the board.

 

with  regards
Harikrishnan R S

.Thank you .

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.