hello
has anyone succeeded to boot from prallel flash using C6727 ?
I followed the instruction on the "using the tms320c672x bootloader" pdf (section 2.2),and I can't manage to boot from flash;
I wrote simple code thats bilnks a led on my board and its running perfectly.
I maped the main function to address 0x10000004(offset 4 at the internal RAM) the execution of the program starts from there according to the pdf (after copying the first 1K from the start of the flash) .
i have burned the first byte on the flash to indicates 16 bit address access (as my flash works) and then i burend my simple program , my flash looked like this:
start flash address -> 0x01010101
my code
It looks like that on startup the dsp do copies the first 1kB from the flash but do not start the execution of the as the pdf asserts .
do you have any ideas?
(i wrote in the past boot for c6713 and it works a little bit different , the dsp generates a reset interrupt after copying the first 1k , according to the mentioned PDF the 6727 does not generates an interrupt but jumps to 0x10000004 and strts the execution from there)