I'm new to the dsp/bios in general, and I' m currently learning how to use the BIOSUSB. I've followed the instructions in the T.I. manuals and I've built the "USB_Dev_Hid" example as it is given in the manuals.
I can build and run the example, however I cannot reproduce the output results as stated in the manual. Also when I run the example (with the usb pluged in) I get the following windows error :
"usb device not recognized."
It looks like something goes wrong during the enumeration of the usb device. By usb device I mean my evaluation board that has a C6748 on-board, which the usb is connected to.
I use:
windows xp,
CCS Version: 4.2.4.00033,
bios_5_41_10_36,
biosusb_01_10_03,
edma3_lld_01_11_02_05,
pspdrivers_01_30_01,
rtfs_1_10_02_32,
xdctools_3_22_01_21,
xdais_7_10_00_06
Has anyone seen this before?