I've purchased an OMAP-L137/TMS320C6747 Floating Point Starter Kit, and  have used c6flo blocks to demonstrate the board with an audio pass through project. I then built a diagram using two square wave generators set to 1 khz, connected to two gain blocks, which were then connected to a stereo audio output. The code generated OK and I successfully built the project for testing on the board. Using cc studio v3.3 I loaded the .out file and ran the program. Using an oscilloscope, I found no square wave present on the audio output jack of the board. Does anyone know where the output can be found? The program runs fine but where's the signal?

Thanks for any help!