I am doing some test dev on the DSK6713 board from spectrum digital. I have developed working code using CCS v3.1 and v3.3 in the past but am trying v5.5 now after a number of years of working on other projects. My question is are there some good resources (videos, books, pdf files, etc) that can help me with this dev? I don't see very much support online or even in books at amazon.com or other sites. Eventually the code will be ported to a C6727 test board then a C6701 final board. I am doing development where I need to have an accurate clock cycle going so I can exercise code at 1 Hz, 5 Hz, 10 Hz etc. I have the POST example working on the C6713 board now, but little else. I also installed the CSL abd BSL libraries but don';t know how to set up a timer or clock accurate program. All the youtube.com videos see to be geared towards CCS v3.1 or v3.3
Thanks,
BG