Hi all,
I am going to work on eye detection and tracking using TMS320C6748 processor. If any body has existing code for this, It will be of great help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I am going to work on eye detection and tracking using TMS320C6748 processor. If any body has existing code for this, It will be of great help.
Hi Ashwith,
Thanks for your post.
I don't think, TI had provided direct example for eye detection but, TI’s new C6748 SYS/BIOS SDK includes several demonstrations for biometric analytics applications, such as fingerprint recognition and face detection, offering a starting point for developing and demonstrating the real-time intelligence of TI’s C674x DSPs.
The SDK also includes the latest SYS/BIOS real-time kernel; the C6748 StarterWare software package, which provides lightweight, operating-system-independent software libraries and utilities; Code Generation Tools; as well as DSP core performance benchmarks that show the real-time processing power of TI’s C674x DSPs.
http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_(LCDK)#Software
Maybe, you can check with IriTech which teams with Texas Instruments on iris recognition camera. Please see the below links:
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------