Hello,
I am using 6748 DSP.
I have two applications which I have built.
I have created an AIS image from each one of them.
As separate application they work just fine. (They are burnt into the NOR flash , each at a time).
What I would like to do is:
Load a SW piece which looks at a certain GPIO.
If the GPIO value is 0 load application1 else load application2
I would like to keep it simple so the applications would be AIS application and let the bootrom load them.
What I cant find is how to make the bootrom logic to go and parse AIS image from a certain address.
I thought maybe to use the AIS jump command or maybe the Software reset option but I couldn’t come out with an answer.
Can someone have an idea?
Thanks,
Eran.