Hello,
I have to interface 512k X32 SRAM to C6727b using EMIF.
So, it needs 19 bit of address . how i have to exactly connect EMIF address and EM_BA pins? and do i need to use GPIO pins also for higher address?
Regards,
Tanisha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have to interface 512k X32 SRAM to C6727b using EMIF.
So, it needs 19 bit of address . how i have to exactly connect EMIF address and EM_BA pins? and do i need to use GPIO pins also for higher address?
Regards,
Tanisha
Hello Tanisha,
Have you selected the SDRAM part per your requirement ?
Could you please share the SDRAM part number ?
As you mentioned, you cannot assume directly the required number of address lines from 512K. The SDRAM addressing is completely different from NOR flash addressing.
The SDRAM comprises row address, column address and bank address. The row address and column address are multiplexed under address lines. The required number of address lines must be available in SDRAM datasheet.
Regards,
Senthil
Hello Tanisha,
The C6727B datasheet specifies (SPRS268E Figure 4.6) that the additional address lines of NOR memory device can be configured using GPIOs.
There is a note, Any GPIO-capable pins which can be pulled down at reset can be used to control A[18:14] for FLASH BOOTLOAD.
I think the same can be implemented for SRAM interface too but not sure about the complexity involved in it.
It seems one of the customer used GPIO bit banging to accomplish this requirement. Please refer below e2e thread for more details.
Regards,
Senthil
Hi Senthil,
I am Sorry but the link you sent is not opening, it says group not found.
I have read about GPIO pins being used as higher address pins but if you can provide some help how to connect it to internal address being generated when i call base address +offset from EMIF, it will be really useful.
I have to connect two external devices SRAM 512k X 32(19 address lines) and EEPROM 128K X 8(17 address lines) on same emif CS2, is it possible and if so both will get CS from EMIF CS or i should use some other pin as i have to distinguish between both when i access it using EMIF?
EEPROM will be used at boot time only, code will be read drom EEPROM and written to SRAm. Later only SRAM will be used for data writing and reading purpose.
Regards,
Tanisha
Hello Tanisha,
The important statement in the given e2e link is below.
Ref: Internal E2E Thread
I believe that your max async memory space is limited by the number of bit-bang GPIO pins that you want to support. Typically, you would create a software layer for memory fetches that will decode the memory address into GPIO bit-bang configurations on the higher address lines and let EMIF handle the lower address lines.
I do not know how to access the internal memory addresses using GPIO and i hope we do not have any example too.
You may search in the internet to get more details about this.
I have to connect two external devices SRAM 512k X 32(19 address lines) and EEPROM 128K X 8(17 address lines) on same emif CS2, is it possible and if so both will get CS from EMIF CS or i should use some other pin as i have to distinguish between both when i access it using EMIF?
In my opinion, you cannot connect two devices on same EMIF CS2.
Regards,
Senthil