Hi there,
This semester we got to work with CCS5 for DSK6713 boards.
I am using CCS v5.2. I have installed the board using the disk provided in the box. was able to successfully upload and run program called sin8_LED provided by disk in the book "Digital Signal Processing and Applications with the C6713 and C6416 DSK". But when I try to run the example of Echo_control and fir4Types, I find no output.
I added all the required C files (namely dsk6713init.C, echo_control.C, Vector_intr.C) library files(rts6700, csl6713, dsk6713bsl, dsk67xx) & header files (dskc6713.h, dsk6713_aic23.h).
I have also changed the input to from line_in to Mic_in. And also changed the the predefined processor as CHIP_6713.
When I build the projects I do not get any errors just a warning about function declared implicitily.
But after I load the program to the board it does not show required output.
I have attached the screen shot of my projects below,
I have attached gel files for both the projects,
Please let me know if you need any further details and help me solve this issue.
Thanks and Regards,
Vanitha