My tms320c6713DSK is failed to connect with my PC,why? I successfully connected it with my PC yesterday ,everything does not change,why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Stifen,
Are you using the internal emulator or external emulator ?
Try to re-connect the USB cable between board and PC .
Check the target configuration of C6713.
Hi Stifen,
Sometimes, these kinds of problem may occur due to reasons such as .... If the user tend to remove the emulator USB cable without stopping the running program at CCS or there is a abrupt power off on target board... e.t.c.
Usually, this will get solved by disconnecting and reconnecting the USB cable on the HOST PC side as well as on the Emulator side and power-OFF and then power-ON the target board.
Regards,
Shankari
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------