I worked on a DSP project before where filter coefficients (coeffs) are listed in the header file (.h) as a single column. Then somehow it is loaded into a array (named BArray) in C/C++ programming, and operations on these coeffs are done based on this array (BArray). However, I couldn't remember how to load these coeffs in the header file into an array in C/C++.