Hi everyone, I had recently bought C6713 and I am planning on using it on my laptop that comes without a CD ROM Drive. I tried downloading the CCS v3.1 but it turns out that it is not compatible with Window Ultimate 7. My question is, during installing of CCS v6.0.1, if i have clicked "Digital Spectrum Driver" does that means that I will not need to run the CD provided by them when I purchased C6713. If I do need additional software, where can I get it other than from the CD ROM provided. Thanks in advance.