Hey,
I've been playing around with the SD card on the LCDkit for the C6748 and am having trouble with booting. I've been using AIS gen to create a bin file for my compiled application and then using SDMMC Writer (included with the C6748 starterware) to load the image onto the SD card on the LCDkit. The board technically boots fine, but I've found the SDMMC Writer (included with the C6748 starterware) blows away the FAT file system on the SD card. How do I load a boot and/or application image and maintain a standard FAT filesystem? I would like to be able to remove my SD card and read it with a standard PC.
Thanks,
Tobyn