Hello:
I want to store 10 16-bit digits into the IRAM of C6713.
The 10 digits are stored in the directive ".mydata".
In my cmd file, I designated the .mydata->MYDATA and the MYDATA is placed at 0x0000202h and the length is 40h.
When I complie, the error occurs like below:
If I change the MYDATA allocation as 0x80000000h and length 0x00000010h. No error would occur.
I think the reason may be if I use IRAM, some spaces in IRAM(I refer to 256kb L2 IRAM) are already pre-occupied or reserved by some
important sections, such as stack far etc.
If I set my MYDATA length as too long, there must be some overlaps between this section and those other internal sections. Is my guess right?
If it is right, how can I check which part of the IRAM has been preempted by those important sections so that I can find my available space? I need to use .map file or some tools of CCSv5?
Thank you