I want to use the C6727B because it has a 32-bit EMIF for asynchronous devices, so I can exchange int32’s and float’s fast so I’ve rule out the C6748.
I have 2 32-bit devices (int32’s & float’s) and 8 8-bit device I need to access. I will set the EMIF for 32-bit and access the 8-bit devices as 32-bit devices no problem I do that now with the VC33.
-
The question I have is about during boot up the parallel NOR flash has to be 8-bit or 16-bit?
-
Can it be flashed for 8-bits and boot up in 32-bit EMIF mode? Or does the parallel NOR flash need to be wired for 8-bit because the DSP need to boot up in 8-bit EMIF mode then switched to 32-bit mode later for normal operation?
Alan