Hi,
I followed all the instructions described in How to Flash Face detect demo on EVMC6748 (processors.wiki.ti.com/.../BIOS_C6SDK_2.0_User_Guide ) Of course I used my AISGen file name and my com port. Everything went just fine, the sfh_OMAP-L138.exe programmed the APP file into the flash. But after I set the DISP switches in LCDKC6748 to boot from the NAND flash memory (and cycled the power) nothing happened. My APP did not run.
I am just guessing why. The only thing what I can imagine is that I needed a lot of RAM memory so my far is set to SHDSPL2RAM in the CMD file:
.far > SHDSPL2RAM
That means – I guess – the entry point of the APP is different than .far would be set to SHRAM. If found the entry point in the release directory MAP file. It is
ENTRY POINT SYMBOL: "_c_int00" address: 8000b4a0
I thought I would try to override the Entry point from the default value to 0x8000b4a0 but when I did it in AISGen then I dropped an error message:
“Cannot specify an entry point without at least one binary file.”
Do you have any idea what’s wrong?
Changing the entry point is a bad idea?
How can run my APP after power on automatically in LCDKC6748 dev. kit?
Thanks