Hi!
I have C6713 DSK and using mcasp example from C6xCSL.
I watch burst on the pins: AHCLKR0 and ACLKR0 on my oscilloscope when I run the program. But on the pins AFSR0 and AFSX0 i have no signals.
What can it be ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I have C6713 DSK and using mcasp example from C6xCSL.
I watch burst on the pins: AHCLKR0 and ACLKR0 on my oscilloscope when I run the program. But on the pins AFSR0 and AFSX0 i have no signals.
What can it be ?
Hi,
Thanks for your post.
Please ensure "csl6713.lib" library search paths below are included in project properties->C6000Linker->FileSearchPath since all CSL API's are included in the CSL libraries:
"~\ti\CSL_C6713\lib_3x\csl6713.lib"
"~\ti\CSL_C6713\lib_2x\csl6713.lib"
For example, "MCASP_enableFsync" is a CSL API which enables internal framesync of the frame sync master. If you put a breakpoint @MCASP_enableFsync and debug, it will let you into the source code of CSL API and you could validate the McASP framesync. Likewise, if you keep breakpoint @InitMcasp(port) and debug, and you could validate the values of AHCLKR, ACLKR through MCASP_ConfigGbl device configuration structure in which, you can check the values of MCASP_PFUNC_AFSX_MCASP, MCASP_PFUNC_AFSR_MCASP and validate the same what it takes. By this, you could narrow down the issue why there is no framesync signals on pins AFSR0 and AFSX0.
May be, you could check the source of CSL API "MCASP_enableFsync" by presuming the CSL_C6713 is installed and you could check the source of CSL from the below paths:
~\ti\CSL_C6713\lib_2x\csl6000.src
~\ti\CSL_C6713\lib_3x\csl6000.src
/*----------------------------------------------------------------------------*/
void MCASP_enableFsync(MCASP_Handle hMcasp, Uint32 direction)
{
Uint32 rfsync = 0;
Uint32 xfsync = 0;
if (direction & MCASP_RCV)
{
rfsync = (MCASP_FMKS(GBLCTL,RFRST,ACTIVE));
}
if (direction & MCASP_XMT)
{
xfsync = (MCASP_FMKS(GBLCTL,XFRST,ACTIVE));
}
if (direction)
MCASP_RSETH(hMcasp,GBLCTL,(MCASP_RGETH(hMcasp,GBLCTL)|rfsync|xfsync));
}
Alternatively, you could also try downloading BSL code examples (dsk6713revc_files.zip) and try McASP example from the below DSK6713 support page:
http://c6000.spectrumdigital.com/dsk6713/revc/
Thanks & regards,
Sivaraj K.
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------
Hi,
Thanks for your update.
Why don't you try BSL McASP example code from DSK6713 support home page which i suggested above?
Do you see the same issue on the BSL sample code too? if not, kindly try and evaluate the frame sync signals on pins AFSR0 and AFSx0.
Keep breakpoints at desired places to debug the code and check why it is not updating AFSR and AFSX from CSL API call "MCASP_enableFsync". Try to narrow down the root cause and check where the culprit is? Try find the code where it got hangs/freezes.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------