Dear Sir:
When I'm running NDK2.0 in TMS320C6747 , it contains a lot of prinf() function , normally it is working properly.
But when I setup a Periodic EDMA transfer (trigged by external interrupt), if the function printf() was called , the EDMA transfer don't work properly. In the CPU Register ,the EMCR and SECR corresponding bit was set to 1, this means that it will never run to the EDMA interrupt routine.
What should I do to avoid this problem?