I would like to send two different outputs to left and right port of lineout /leftout.
Can you kindly let me know how to should i program the device to do that.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to send two different outputs to left and right port of lineout /leftout.
Can you kindly let me know how to should i program the device to do that.
Hi,
Thanks for your post.
The TLV320AIC23B has line inputs for the left and the right audio channels (RLINEIN and LLINEIN). Both line inputs have independently programmable volume controls and mutes.
The TLV320AIC23B has stereo headphone outputs (LHPOUT and RHPOUT) and The DAC outputs, line inputs, and the microphone signal are summed into the line outputs. These sources can be switched off independently. All these needs to be configured appropriately in proper operating modes through AIC23 codec set of registers which can be reviewed through codec datasheet as below:
http://www.ti.com/lit/ds/symlink/tlv320aic23b.pdf
Please check sections 3.2.1, 3.2.2, 3.2.3, 3.2.4 from the above datasheet.
Also, please check the below E2E post to program the AIC23 codec for the left and right inputs:
https://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/215800#pi317286=2
while (1) {
/* Read sample from the left channel */
while (!DSK6713_AIC23_read(hCodec, &IN_L));
/* Feeding the input directly to output */
OUT = 500*IN;
while (!DSK6713_AIC23_write(hCodec, OUT_R));
}
/* Close the codec */
DSK6713_AIC23_closeCodec(hCodec);
}
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------
Hi,
I would reecommend you to go through the lab doc as below which involves programming the TMS320C6713 DSP Starter Kit (DSK) module:
http://ecee.colorado.edu/~fmeyer/class/ecen4532/lab6.pdf
You can also find a simple program from
Wiki: processors.wiki.ti.com/.../File:C6713_audio_minimal.zip
You could also download the board support files from specturn digital webite on the prerequisites on the wiki below:
processors.wiki.ti.com/.../C6713DSK_in_CCSv5
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------