Hi,
I have been working the device DSK6713. I would like tot know , how to generate a sine wave of required frequency and amplitude on CCS. I tried to pregenerate the sine wave values using Matlab and add that to table. But i couldn't figure out how to convert the matlab values to CCS. SO is there any way we can produce the sine wave
these are the MATLAB Values i got,
Columns 1 through 9
0 0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511
Columns 10 through 18
-0.5878 0.0000 0.5878 0.9511 0.9511 0.5878 0.0000 -0.5878 -0.9511
Columns 19 through 27
-0.9511 -0.5878 0.0000 0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878
Columns 28 through 36
-0.9511 -0.9511 -0.5878 -0.0000 0.5878 0.9511 0.9511 0.5878 -0.0000
Columns 37 through 45
-0.5878 -0.9511 -0.9511 -0.5878 0.0000 0.5878 0.9511 0.9511 0.5878
Columns 46 through 54
-0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000 0.5878 0.9511 0.9511
Columns 55 through 63
0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878 -0.0000 0.5878 0.9511
Columns 64 through 72
0.9511 0.5878 0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000 0.5878
Columns 73 through 81
0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000
Columns 82 through 90
0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878
Columns 91 through 99
0.0000 0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511
Columns 100 through 108
-0.5878 0.0000 0.5878 0.9511 0.9511 0.5878 0.0000 -0.5878 -0.9511
Columns 109 through 117
-0.9511 -0.5878 0.0000 0.5878 0.9511 0.9511 0.5878 0.0000 -0.5878
Columns 118 through 126
-0.9511 -0.9511 -0.5878 -0.0000 0.5878 0.9511 0.9511 0.5878 0.0000
Columns 127 through 135
-0.5878 -0.9511 -0.9511 -0.5878 -0.0000 0.5878 0.9511 0.9511 0.5878
Columns 136 through 144
-0.0000 -0.5878 -0.9511 -0.9511 -0.5878 -0.0000 0.5878 0.9511 0.9511
Columns 145 through 153
0.5878 0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000 0.5878 0.9511
Columns 154 through 162
0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000 0.5878
Columns 163 through 171
0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878 0.0000
Columns 172 through 180
0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511 -0.5878
Columns 181 through 189
0.0000 0.5878 0.9511 0.9511 0.5878 -0.0000 -0.5878 -0.9511 -0.9511
Columns 190 through 198
-0.5878 -0.0000 0.5878 0.9511 0.9511 0.5878 0.0000 -0.5878 -0.9511
Columns 199 through 201
-0.9511 -0.5878 0.0000