Dear All
We have designed a board based on smj320c6701. The board contains a 32 bit boot flash in 32 bit room boot mode map0. We already had successfully developed a board with Tms320c6701. In its next version, we only changed the DSP from TMS to SMJ. The board fails in booting intermittently, especially if it is powered off for longer periods of time. If we connect the emulator when the board fails to boot, the internal registers and rams are accessible but external rams and flash are inaccessible. The contents of external rams are almost identical (Most of memory locations have same values when seen in CCS 3.0 IDE). We used a scope and observed that the processor was generating the CS1 chip select for flash during boot but some how the data loaded on address 0 is not the correct one.
The data sheet of processor does not suggest power sequencing. More over, the core and IO supply power up almost at the same time.
Kindly advise on this issue.
Thanks
Ahsan Shabbir