Hello TI,
On the TMS320C6748 EMIF bus it is possible to natively address a 16-bit device up to 32MB by connecting A[22:0]+BA[1] to the 16-bit device's A[23:0], as indicated in most TI examples.
However, spruh79a states on page 776: Additionally, when the EMIFA interfaces to a 16-bit asynchronous device, the EMA_BA[0] pin can serve as the upper address line.
This seems to indicate that connecting BA[0]+A[22:0]+BA[1] to a 16-bit device's A[24:0] is plausible, thereby natively addressing up to 64MB (ie. without additional GPIOs for the MSBs, Bank selects or additional logic or BA[0] being used as GPIO).
Is this true, or what does the sentence otherwise refer to, spruh79a specifically being the Technical Reference Manual for the TMS320C6748 DSP after all?