Hi
I am using tms320c6713 evm board. I want to flash burn for my final project. When i have tried with my sample LED program as per TI guide-line. it is working correctly. But when i want to flash burn with my own project program , during .cmd to .hex convertion by hex6x.exe through command prompt , it show the warning message and burning .hex code is not worikng. If i implement simple program for flash burn and by .hex convertion process, have not shown this type of warning, it is working fine.
my warning meassages are:
WARNING: section '.text' at 03000h falls in unconfigured memory (skipped)
WARNING: section '.cinit' at 085a0h falls in unconfigured memory (skipped)
WARNING: section '.const' at 0a36ch falls in unconfigured memory (skipped)
WARNING: section '.switch' at 0a6b0h falls in unconfigured memory (skipped)
like this. How to fix the warning and what are the exact meaning of this warning.
My .cmd file configuration is shown below.
/*C6713dsk_flash.cmd Linker command file for flash*/
MEMORY
{
VECS: org = 0h, len = 0x200
BOOT: org = 0x00000200, len = 0x200
IRAM: org = 0x00000400, len = 0x0002FB00
SRAM_EXT: org = 0x80000000, len = 0x01000000
FLASH: org = 0x90000000, len = 0x00020000
}
SECTIONS
{
"bootload" :> BOOT /*boot section.Runs when C6713 starts*/
.vecs :> VECS
.text :> IRAM
.bss :> IRAM
.cinit :> IRAM
.stack :> IRAM
.sysmem :> IRAM
.const :> IRAM
.switch :> IRAM
.far :> IRAM
.cio :> IRAM
.csldata :> IRAM
}
If any body know the solution , kindly help me.
Wait for your kind response.