Hi
My customer wants to know the side effect when specifying SDTIMR2.T_RTP with larger value than 1.
A spread sheet for DDR configuration is available from the following link:
And it says SDTIMR2.T_RTP should be configured with 1 when using mDDR.
Currently, my customer is using mDDR and has configured it with 3 in their development phase. And so far they don't see any problems in DDR access.
Do you think we can leave it 3 ?, or Should we use 1 as a spread sheet suggested ?
Best Regards,
Naoki Kawada