Hi.
My customer reported that the VTPIO_CTL value is 0x0018E1B7 after the C6746 UART boot. The bit 6 (POWERDN) of it is 0. He assumes that POWERDN should be set by the ROM bootloader at the end of the VTP IO calibration. Is the 0 of the POWERDN bit normal? And does he need to set the bit with an user code to save power? Or does the ROM bootloader fail to initialize the DDR2?
Best regards,
Tsutomu Furuse