hello,
I use c6701, flash is 16 bit wide, and is in CE1, I configure the dsp boot as 10101 MAP 1 Internal 16-bit ROM with default timings; but the CE Space Control Register MTYPE bit field is set as MTYPE = 010b: 32-bit-wide asynchronous interface when dsp power on.
I want to make sure whether my BOOT pin configuration is right. Or I should set the dsp boot pin as 11101 MAP 1 Internal 32-bit ROM with default timings?
Best Regards,
Si