Hi,
I am using LCDK c6748, getting idea from the earlier post, I have converted 512x512 bmp image into a header file, but the converted file is too big and puts the CCSv6 to unresponding mode. So, I resize the image to 64x64, but the converted header file when used in raster display example from starterware does not display the image on LCD.
So, I jump to another utility bmp2c, but the converted format is not compatible with the code, it shows error as....
IMAGE_FMT_16BPP_UNCOMP is undefined
I wanted to know what this identifier is and where it has to be defined, so that I can use the converted raw data with raster example.Also, the pixel values are not in 16 bit format, they are in 8 bit format.
The raster example as provided in starterware has an array of raw data which displays starterware image on the LCD, how can I display any bmp image using raster example?
Regards
Rohit