Hi,
When downloading TMS320C6743 via UART0 I've been using:
- *.out file working on board with JTAG (test application with flashig led)
- AISgen for D800K005 version 0.8.2.0
- UART Boot Host Utility (both from sprab04g.zip installation)
I've experiened a problem to complete downloading the application:
The questions are:
1. What's going wrong?
2. Is there document with detailed description of AIS commands?
Please, hint me the best way to successfully download and start program on TMS320C6743 (D800K005 ROM).
I have trying UART0 boot because of NAND8 boot still does't work. And UART0 boot utility has some logging info.