Hi,
When I'm trying to boot C6743 from NAND 8-bit, it does't work.
NAND device is in supported NAND devices list (ID 0x75) - NAND256W3A2BZA6E.
I'm using working *.out file, AISgen utility, and application tested on UART0 boot.
The only change I made is selecting NAND 8-bit instead UART0.
I have read sprabb1c and (as was recommended in my previous post - spra04g).
I'm burning *.bin file to the NAND starting from block 1 page 0.
NAND is connected to DSP according sprabb1c:
NAND Flash should be connected to EMA_CS[3] of the EMIFA peripheral. The ALE and CLE pins of the NAND device should be connected to the EMA_A[1] and EMA_A[2] pins of the EMIFA peripheral, respectively.
My program do not use first 16kB L2 RAM as recommended in sprabb1c:
Memory Usage: The bootloader uses 16 KB of DSP L2 RAM starting from 0x11800000 for multiple purposes. This memory should not be used by any initialized section of the user application.
It should be noted that on C6743 the memory map slightly differ from C6747: L2 RAM resides addresses from 0x11820000 - 0x1183FFFF,
as described in sprs565d.
Test bytes of each page is 0xFF, 10 ECC bytes are programmed.
The access to the NAND is performed, that I can see on oscilloscope attached to corresponding pins.
What may be wrong?
Thanks in advance for any ideas!