Hi,
Setup: TMS320C6748, XDS200 and CCS 6, USB thumb drive, powered USB HUB, USB Card Reader, SD Card
Goal: I would like to write a simple code to read files from the USB thumb drive and write it to the SD Card.
Skills: I am a complete newbie with CCS and DSP programming.
1) Since the TMS320C6748 only has one USB port, I've got a powered hub to connect the two different types of drives, is this setup acceptable?
2) What packages do I need to achieve this?
3) Does the DSP/BIOS and SYS/BIOS provide a similar Linux filesystem that let's me recognize the drives, do a directory listing of the files, read/write files?
4) What the API's for doing this? Are there examples?
Any links to the API and examples would be very helpful as I am brand new. I've got the hello world to work and the LED demo to work so now ready to try communicating to the drives. I have not connect the drives. I'm waiting to hear if my setup is ok.
Thank you in advance for any help.