Hi,
I am just beginner of CCS and DSP, my Programm entain contain a lot of data wich are need to be inputed and oututed. The default length of IRAM is not enough. I need about double size of the default length of IRAM. I am not sure is there enough RAM in the board, I read in the technical reference that there is also a great quantity of Memory of EMIF, but I dont know if I can use this area to save all the sections or I can only save part of the Programm in this area?
And if I can save my Programm in this area, what should I do to change the storage location of the Programm. Should I change the memory location in the Link File (c6713.cmd)?
Any suggestions/recommendations/information on the above will be greatly appreciated.
Regards...